Target_Velocity
| Index.Sub | 60FF.0H |
| Data Type | Integer32 |
| Access | Read/Write |
| PDO Mappable | RX_PDO (1) |
| Unit | User-defined velocity unit (2) |
|
Range |
0 to Max_Profile_Velocity (607F.0H) |
| Default Value | 0 |
| Store Supported | No |
| Description | This object indicates the configured target velocity. It is used in Profile Velocity mode (pv) and Cyclic Synchronous Velocity mode (csv). |
|
Notes |
(1) available with firmware V00r74 or superior. (2) See Factor Group. |